DOCA0260EN-00

Disable Unused Ports/Interface

Disabling unused ports/interface helps reduce the system’s attack surface by turning off communication ports and interfaces that are not actively used.

The following settings of the TeSys Tera system can be disabled using the standard web server:

  • Modbus TCP

  • Device Dicovery

  • Modbus RTU

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?