DOCA0260EN-00

Decommissioning

The TeSys Tera system contains confidential information configured during commissioning, recent data values, and logs.

For example, this information can include Modbus LTMT main unit topology, or measured power consumptions.

It is required to perform a factory reset before disposing of the TeSys Tera system.

You can use the following ways to reset the TeSys Tera system:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?