DOCA0275EN-02

Installing SoMove

Overview

SoMove software is a Microsoft Windows® based application, using the open FDT or DTM technology. SoMove software contains multiple DTMs.

Downloading SoMove Software

SoMove software can be downloaded from Schneider Electric website.

NOTE: You must have administrator rights to download, install, or uninstall the software on your PC.

Installing SoMove Software

The following steps describe how to install SoMove software:

  1. Unzip the downloaded file SoMove_FDT.

  2. The folder will contain an .exe file named SoMove _VX.Y.Z (where X.Y.Z is the version number) and a release note.

  3. Double-click SoMove _VX.Y.Z to start the installation.

  4. In the Choose Setup Language dialog, select the installation language.

  5. Select OK.

  6. In the Welcome to the Installation Wizard for SoMove dialog, select Next.

  7. If an Install Shield Wizard dialog appears and informs you that you must install Modbus driver, select Install.

    Result: Modbus driver is installed automatically.

  8. In the Readme and Release Notes dialog, select Next.

  9. In the License Agreement dialog:

    1. Read carefully the license agreement.

    2. Select I accept the terms in the license agreement option.

    3. Select Next.

  10. In the Customer Information dialog:

    1. Enter the following information in the corresponding fields:

      • First name

      • Last name

      • Company name

    2. Select Next.

  11. In the Destination Folder dialog:

    1. If necessary, modify the SoMove software destination folder by selecting Change option.

    2. Select Next.

  12. In the Shortcuts dialog:

    1. If you want to create a shortcut on the desktop and or in the quick launch bar, select the corresponding options.

    2. Select Next.

  13. In the Ready to Install the Program dialog, select Install.

    Result: The SoMove software components are installed automatically with:

    • Modbus communication DTM library which contains the communication protocol.

    • DTM libraries which contain different catalogs.

    • SoMove software

  14. In the Installation Wizard Completed dialog, select Finish.

    Result: SoMove software is installed on your PC.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.