Terminal Shield

Terminal shields can be installed on the top and/or bottom of the power terminals of transfer switching equipment to provide IP20 protection.

NOTE: The terminal cover and the terminal shield cannot be used together.

The table below provides the list of the terminal shield:

Switch

Number of poles

Terminal shield

Frame 100: 32–100 A

4P

TPSISO30

Frame 160: 80–160 A

4P

TPSISO31

Frame 250: 100–250 A

4P

LV429518

Frame 630: 320–630 A

Frame 800: 800 A

4P

TPSISO42

For information on installation, consult the instruction sheets on Schneider Electric website:

  • TransferPacT Active Automatic / Automatic 32-100 A:

    JYT3049801

  • TransferPacT Active Automatic / Automatic 80-160 A:

    JYT3049901

  • TransferPacT Active Automatic / Automatic / Remote 100–250 A:

    GEX2525501

  • TransferPacT Active Automatic / Automatic / Remote 320–630 A:

    GEX2525601

  • TransferPacT Active Automatic / Automatic / Remote 800 A: BQT1751501

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?