BUS Extension and 24 VDC Auxiliary Supply

The BUS extension and 24 VDC auxiliary supply is an accessory module installed on TransferPacT Active Automatic controller with following functions:

  • Bus extension, 1 RJ45 is provided.

  • DC 24 V and 1 input is provided.

  • Green LED on the front face of the accessory indicates the power status and proper connection of the accessory.

  • Communication with the main MCU on ATSE.

  • Only one BUS extension and DC 24 V auxiliary supply is allowed to be installed on one product, in the right most slot.

Application BUS Extension

BUS extension is used to connect external HMI.

Application with DC 24 V

  • External power for controller when both source failure.

  • External power to keep power for Modbus communication when both source failure.

Terminals

For BUS Extension

  • RJ45

DC 24 V

  • 24 V+, 24 V-

Signal Type

Power supply and bus extension.

Performance

Electrical characteristics

Ratings

Ui

30 V DC

Maximum Input voltage

28.8 V DC

Minimum input voltage

19.2 V DC

Maximum input current

1 A

Pollution degree

3

Altitude

2000 m

RJ45

CAT 3

Cable Capacity for Terminals

The cable capacity for the terminals are as below:

  • The cable capacity for the terminals are 0.05 – 2.6 mm2 (AWG 30 ~ 13).

  • RJ45

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?