Threshold

Description

Settings

Default setting
% of nominal

Adjustment range

Note

Voltage

Delta Dropout (under and over voltage)

10%

4 -> 20%

Step of 2%

Delta Pickup

20% of delta drop out

fixed

fixed

Frequency

Delta Dropout

5%

2 -> 10%

Step of 1%

Delta Pickup

20% of delta drop out

fixed

fixed

The accuracy of voltage sensing is 1%.

The accuracy of frequency sensing is 0.1%.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?