Weights

This section describes the weights of the TransferPacT Automatic, TransferPacT Active Automatic and TransferPacT Remote switches.

Frame ratings

Weights

Frame 100: 32– 100 A

3.4 kg

Frame 160: 80– 160 A

5.6 kg

Frame 250: 100– 250 A

13.3 kg

Frame 630: 320– 630 A

22.1 kg

Frame 800: 800 A

22.4 kg

Frame 1A: 800– 1250 A

69 kg

Frame 1A: 1600 A

72.3 kg

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?