Equipment Description

TransferPacT Active Automatic / Automatic 32-100, 80-160 A

TransferPacT Active Automatic / Automatic / Remote 100–250, 320–630, 800 A

TransferPacT Active Automatic 800-1600 A

Label

Description

A

Position for HMI modular

B

Active Automatic HMI (with LCD display)

C

Automatic HMI (with rotary switch)

D

Slots for function module

E

Power connections

F

Position indicator

G

3- position slider: Auto/Manual/Lock

H

Single line diagram

I

Dielectric switch

J

Protective earth

K

Carrying grip

L

Spring charged and ready-to-open indicator

M

Spring charged handle

N

Source II push button

O

OFF position push button

P

Source I push button

Q

Mounting side plate

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?