Remote Transfer

The remote transfer is a fixed function for TransferPacT Remote with following functions:

  • Remote transfer is an active input. It can transfer the TSE to source I or source II or OFF position according to input signals. There’s no time delay, no source detection for remote transfer.

  • Customer should give a rising edge signal, and keep the signal for no less than 200 ms to start remote transfer.

Electrical wiring

Terminals

There are 4 terminals of the remote transfer function as below:

  • R0-R1: Remote to SI

  • R0-R2: Remote to SII

  • R0-R3: Remote to OFF

Signal type

  • Digital input with dry contact.

  • Need over 200 ms input to start remote control.

Cable Capacity for Terminals

The cable capacity for the terminals are 0.5 – 2.5 mm2 (AWG 24 ~ 12).

Maximum cable length: 10 m

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?