DUG_IR Converter_WASIA-01

Adding IR controlled devices

Add infrared-controlled appliances such as televisions, split system air conditioners, and music systems to an IR Convertor and control them using the app.

IMPORTANT: If you have a brand-new model of TV, split system air conditioners or HiFi system, the IR code sets may not yet be available in the IR Convertor. The code sets in the IR Convertor are updated regularly, but there may be times when a new model appliance cannot be used with the device.

NOTE: This task uses the example of adding a television to the IR Convertor. The same method can be used to add other infrared-controlled appliances such as split system air conditioners and HiFi systems.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?