DUG_IR Converter_WASIA-01

Changing the device icon

Using the Wiser app, you can change the icon of the device.
Follow the steps to change the device icon:
  1. On the Home page, tap All devices > IR Convertor.
  2. Tap icon and tap .
  3. Tap Icon to view the menu.
  4. In the slide-up menu, select any one of the following (A):
    • Take photo - Allows you to take a photo from the mobile camera
    • Select from Icon Library - Allows you to select an icon from the app library
    • Select from Album - Allows you to select photo from the mobile gallery

  5. Tap on the required photo/icon to change the icon.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?