DUG_IR Converter_WASIA-01

Replacing the battery

Replace the device battery when the level is low or critically low. The battery level can be seen in the app.

To replace the battery from the device:

WARNING
CHEMICAL BURN HAZARD
Keep batteries out of reach of children. If swallowed, seek immediate medical attention.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTICE
PERFORMANCE DEGRADATION OR EQUIPMENT DAMAGE
• The device should be powered only by the provided AC adaptor or 4× AA batteries.
• Only alkaline batteries should be used. Do not use rechargeable batteries.
Failure to follow these instructions can result in equipment damage.

  1. Rotate the module by 70° clockwise to separate the device from the back cover.

  2. Replace the batteries with proper polarity.

  3. Position the module to the cover and rotate 70° anti-clockwise.

    NOTE: Dispose the used batteries, as per statutory regulations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?