DUG_Wireless PIR dimmer_LK-00

About the device

The Wiser wireless PIR dimmer with neutral (hereinafter referred to as Motion sensor dimmer) detects moving heat sources (e.g. persons) and can dim ohmic, inductive or capacitive loads and switch them on for a settable overtravel time.

Control options

Home control: To control the motion sensor through the Wiser app you will need the Wiser Gateway / Hub.

Direct operation: The motion sensor can always be controlled directly on-site. You can also connect any number of mechanical push-buttons to control the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?