DUG_Wireless PIR dimmer_LK-00

Sensor setting

Sensitivity Setting

Using the Wiser app, you can set the sensitivity of the sensor (such as High, Medium, Low).

Tap Sensitivity Setting and select one of the following levels (A):

  • High

  • Medium

  • Low

NOTE: The high sensitivity level detects the slightest movement.

Detection Delay

Using the wiser app, you can set the detection delay time.

Tap Detection Delay and select the time duration (B) or tap Detection delay custom (C) to customize your detection delay time.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?