DUG_Wireless PIR dimmer_LK-00

Lux Customization

Using the Wiser app, you can define the threshold value for lux ranges (such as very dark, dark, bright, very bright) of the environment. This will help to prevent the false alarm caused by changes in the light intensity.

Tap Lux Customization and drag the slider bar (A) to define its threshold value and tap Confirm.

  • Very dark level - Lux value ranges from 1 lux to 100 lux

  • Dark level - Lux level ranges from 6 lux to 300 lux

  • Bright level - Lux level ranges from 101 lux to 2000 lux

NOTE: The Current Lux Value is the current light level present in the environment measured by the sensor.

Example: If Lux Customization is configured to 500 lux, if the current lux is less than 500lx and there is movement, then the load will turn on, and if the current lux is more than 500lx and there is movement, then the load will not turn on.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?