Dimmer setting
Dimming Mode
You can change the dimming mode in the app if you have problems with light flickering. This improves the dimming quality.
Tap Dimming Mode and select either of the following (A):
– Auto - When any other load is connected to the dimmer (e.g. filament bulb).
– RL-LED - When a LED is connected to the dimmer.
Dimming Range
You can restrict the maximum and minimum brightness of the load connected to the device. This is done to avoid flickering and switching off the LED.
Tap Dimming Range and do either or both of the following (B):
– Min Brightness - Drag the sliding bar to restrict the minimum brightness.
– Max Brightness - Drag the sliding bar to restrict the maximum brightness.
Toggle mode setting
Using this setting, the device will remember the last state of the device.
Tap Toggle Mode Setting and select any one of the following (C):
– 100% - The LED glows at maximum brightness every time it is turned on.
– Last Level (Memory Function) - The LED glows at the previously set brightness level whenever it is turned on.