DUG_IPC_Outdoor_LK-02

About the device

The Wiser IP camera outdoor (hereinafter referred to as IP Camera) is a Wi-Fi® operated device that is used to monitor sensitive outdoor areas of your home with a HD recording. You can install the camera indoors or outdoors in all directions (e.g. on the wall, under the roof, etc.). The IP camera can be triggered by other Wiser devices (such as sensors).

Advantages of using an IP camera:

  • Increases your overall safety

  • High resolution recording

  • Covers a wide area

  • Infrared night vision for low light recording

NOTE: Users are solely responsible for adhering to applicable privacy laws, e.g. the GDPR, Article 5. Users must ensure that guarantees are taken to avoid any misuse of equipment for surveillance or entirely different and unexpected purposes than intended.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.