DUG_IPC_Outdoor_LK-02

Inserting a micro-SD card

The micro-SD card is inserted in the device to store the recording.
NOTE: The micro-SD card has to be inserted before you power on the device. If the device is already turned on, then turn off the device to insert the micro-SD card.

Follow the steps to insert a micro-SD card:

  1. Remove the lid on the back of the camera.
  2. Insert a micro-SD card in the memory card slot.
  3. Close the lid.
    Once the micro-SD card is inserted, you can configure the playback settings.
    NOTE: A maximum of 128 GB SDHC and SDXC micro-SD cards with FAT32 format are supported.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.