DUG_IPC_Outdoor_LK-02

Playback

Using the Wiser app, you can review the recording whenever you want with the Playback feature.
NOTE: You need to insert a micro-SD card (max 128 GB) to use the playback feature.

The control panel of the playback consists of:

Select the recording date and time

Click screenshot of the video

/

Pause/play the recording

Record the video

NOTE:
  • A display screen on the control panel shows the previous recordings.

  • The screenshot/recording will be saved in the album.

Recording settings

Follow the steps to change the recording settings:

  1. On the Home page, tap All devices > IP Camera Outdoor.

  2. Tap and tap Settings > Recording Settings.

  3. In the Recording Settings section, tap the toggle switch (A) to enable the Local recording.

    NOTE: The recording will be saved to the micro-SD card.
  4. Tap Recording mode (B) and select one of the options:

    NOTE: Recording mode is enabled only when you turn on the Local recording toggle switch.

    Event recording - Records only when there is a motion detection

    Non-stop - Records continuously for 24 hours

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.