DUG_IPC_Outdoor_LK-02

Setting privacy zone

The Privacy Zone settings allows you to set the surveillance area for monitoring on the live view.
Follow the steps to set the privacy zone:
  1. On the Home page, tap All devices > IP Camera Outdoor.
  2. Tap and tap Settings > Privacy Zone.
  3. Tap the toggle switch (A) to turn on the Privacy Zone.
  4. Tap Surveillance area setting (B) and drag/resize the red frame to set the surveillance area and tap Save.
    The live view on the control panel will show only the saved surveillance area.
    NOTE: The privacy zone detection area setting overrides the motion detection activity area setting. Therefore, even if the motion detection activity area is larger than the privacy zone detection area, the motion will only be detected within the privacy zone detection area.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.