DUG_Sedna-Motion Sensor_WSE-00

Creating a schedule

The Motion Sensor Switch can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.
  1. On the Home page, tap All devices > Motion Sensor Switch.
  2. Tap Schedule > Add schedule to add a schedule.
  3. Set the time (A).
  4. Tap Repeat (B) to select the days you want to set the schedule.
  5. Tap Note (C), enter the note and tap Confirm.
  6. Tap the toggle switch to turn on the Notification (D) for the schedule. The app will send a notification that the scheduled task is executed at the time of schedule.
  7. Tap Motion Relay (E) and select one of the options:
    • On - Turns on the Motion Sensor Switch on the scheduled time
    • Off - Turns off the Motion Sensor Switch on the scheduled time

  8. Tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?