DUG_Sedna-Motion Sensor_WSE-00

Example of an automation

This demonstration shows you how to create an automation to switch on the motion sensor switch at the scheduled time.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name , enter the name of the automation and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping .
  3. Tap Add Condition > Schedule.
    • Tap Repeat (A), select the days you want to set the schedule and tap Save.

    • Set the time (B) at which the automation must start and tap Next.

  4. Tap Add task > Run the device > Motion Sensor Switch.
  5. Tap Motion Relay > On and tap Save.

  6. Tap Next.
  7. In the Automation Settings page, tap Save.

    Automation is now available under Automation tab. Use toggle switch to enable/disable automation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?