DUG_Sedna-Motion Sensor_WSE-00

Resetting the device

You can reset the device to factory default manually.
To reset the device:
  1. Short press push button three times (< 0.5 s) and then long press the push button once (>10 s).
  2. After 10 s, LED starts blinking red then release the push button.
    The LED stops blinking upon successful reset of the device.
  3. The Motion Sensor Switch restarts and blinks green for a few seconds.
    NOTE: After reset, the LED turns amber.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?