DUG_Sedna_FLS_WSE–01

Unbinding a moment

Unbinding the moment allows you to remove the moment from the assigned keys without deleting the moment.
  1. Go to the control panel and tap Top right key.
  2. Tap Unbind.
  3. Short press the top right push button 3 times on the Wireless Switch to activate the device and tap Confirm on the app.

    The moment is now removed from the top right key.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?