DUG_Sedna_FLS_WSE–01

Changing the device from 1-gang to 2-gang

You can change the Wireless Switch mode from 1-gang to 2-gang before you pair your device to the Gateway.
NOTE: The Wireless Switch is in 1-gang mode by default.
Follow the steps to change the mode:
  1. Remove the 1-gang rocker from the module.

    NOTICE
    Module damage
    The module is locked into the rocker. Use a screwdriver and carefully remove the rocker from the module.
    Failure to follow these instructions can result in equipment damage.
  2. Mount the 2-gang rocker on the module.

  3. Insert the module into the frame from the front and ensure that it clicks into place.

  4. Press and hold the top right and bottom left push button simultaneously for 10 seconds until the LED starts blinking red.

    The red LED indicates the switching process. The Wireless Switch is now changed to 2-gang mode.

NOTE: To change the mode back to 1-gang, reset the device and replace with 1-gang rocker.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?