DUG_Sedna_FLS_WSE–01

About the device

The Connected Wireless Switch 1-gang/2-gang (hereinafter referred to as Wireless Switch / Freelocate Switch) is a battery-powered wireless switch that is used to control a group of Zigbee devices (such as light and shutter) within the same Zigbee network. The device can be configured through the Wiser app.

Features of the Wireless Switch:

  • Add a Group (such as lighting and shutter control).

  • Add a Moment (such as Movie Night, Good Night Moment).

  • Low battery notification.

NOTE:
  • This device user guide shows pairing, configuring and other features of Wireless Switch 2-gang. The same applies for Wireless Switch 1-gang.

  • Construction materials may cause interference which affect Gateway-to-device and device-to-device distances. In the open air, there is no interference, so the distance can be much longer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?