Device user guide_03

Calibration

The shutter control is supplied in an uncalibrated state. Each shutter motors vary in the speed at which they open and close (edge to edge). Therefore, the opening/closing time of the shutter must be determined in the app.
NOTE:
  • Before using this device for the first time, it must be calibrated, or you can adjust its duration manually.

  • Do not use the shutter either manually or on the app during calibration to avoid interruption.

Shutter calibrating


To calibrate the run time manually:

  1. On the device control panel page, tap Settings > Open/Close Duration.

  2. On the slide-up menu, you can set the run time manually using +/- button or using the sliding bar (A) and then tap Confirm.

    NOTE: To determine the default run time, record the time it takes to fully open/close the shutter (edge to edge).


To calibrate the run time using app:
  1. In Settings > Open/Close Duration, tap Calibration (B).

  2. On the slide-up menu, select the calibration start point (C):
    Start from the top: The shutter will move from top to bottom (closing).
    Start From the bottom: The shutter will move from bottom to top (opening).

  3. Wait until the shutter reaches its starting point and then tap Start.

  4. Tap Done (D) once the shutter reaches other end.


    The app displays the progress of calibration.
  5. Once the process is complete, tap Tilt Calibration on the pop-up window for shutter slat calibration.

Slat tilt angle calibration

To calibrate slat tilt angle:

  1. On the Settings page, tap Slat Tilt Angle for slide-up menu.

  2. Select tilt type (A) based on the motor installed and then tap Confirm:

    • 90 Slat Rotation

    • 180 Slat Rotation

    • Not Supported

    • Blind

    IMPORTANT: If the shutter is installed with a non rotating slat or blind, the calibration process is complete, and no further steps to follow.
  3. Read the pop-up notification and tap Confirm.

  4. Make sure the shutter is in fully closed state and tap Prepare.

  5. Select the check box (B) and tap Start.

  6. Tap Stop (C) to finish calibration.

    TIP: You can retake the calibration by tapping Reset.
  7. Tap Done once the process is complete.


    The app displays the progress of calibration.
    TIP: You can set the run time manually by taping
    Duration Adjustment (D).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?