Device user guide_03

Operating the device using app

By using the Wiser app, you can open\close the blind.
  1. On the Home page, Tap All devices.
  2. On Blind Control Switch, tap ˅ for common function.
  3. On the slide up Control menu, select Open/Close to operate the shutter.

  4. Alternatively, you can navigate to the control panel of the device to preform the operation.
    NOTE: The control panel shows the current state of the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?