Device user guide_03

Using the device

The Control Panel allows you to open/close, increase/decrease the height of shade and control various settings.

On the Home page, tap All devices > Blind Control Switch to access the control panel.

On the control panel page, you can see the following:

  • The current state of the device (A)

  • Control button (B)

  • Slat position control (C)

  • Schedule (D)

  • Settings (E)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?