DUG_Unica Rotary dimmer_WSE-03

Switching/Dimming the device using app

Using the Wiser app, you can switch On/Off and increase/decrease the brightness of the device.

Switch On/Off the device

To switch on/off the device:

  1. On the Home page, tap the power button (A) to turn on/off the Rotary Dimmer.

  2. Alternatively, you can navigate to the control panel of the device and tap to turn on/off the Rotary Dimmer.

    NOTE: The control panel shows the current state of the Dimmer.

Adjusting the brightness of the device

To increase/decrease the brightness of the device:

  1. On the Home page, next to device name, tap the ˅ and drag the slider to adjust the brightness of the Dimmer.

  2. Alternatively, you can navigate to the control panel of the device and drag the sliding bar up/down to increase/decrease the brightness.

    NOTE: The control panel shows the current brightness percentage of the Dimmer.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?