DUG_WSE_IPC_Outdoor_02

Configuring basic function settings

The basic function settings allows you to enable the Status indicator on the device and the Time watermark on the Wiser app.

Status indicator

Enabling the Status indicator turns On/Off the LED on the device.

Follow the steps to enable the Status indicator:

  1. On the Home page, tap All devices > IP Camera Outdoor.

  2. Tap and tap Settings > Basic function settings.

  3. Tap the toggle switch (A) to enable the Status indicator.

NOTE: The LED indicates blue on the device when the status indicator is turned On.

Time watermark

Enabling the Time watermark displays the date and time on the live view on control panel.

Follow the steps to enable the Time watermark:

  1. On the Home page, tap All devices > IP Camera Outdoor.

  2. Tap and tap Settings > Basic function settings.

  3. Tap the toggle switch (B) to enable the Time watermark.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?