DUG_WSE_IPC_Outdoor_02

Setting image quality

Using the wiser app, you can change the image quality based on your requirement.
TIP: You can switch to Standard Definition image quality when the Wi-Fi is slow or the memory card storage space is less.
  1. On the Home page, tap All devices > IP Camera Outdoor.
  2. Tap and tap Settings > Image Quality.
  3. Select any one of the options:
    • Standard Definition (SD) - Captures low resolution video/image
    • High Definition (HD) - Captures high resolution video/image

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?