SUG_Wiser_Home_Iberic_WH-05

Energy Domain without Grid

You can monitor your energy consumption and production even without a grid monitoring device (PowerTag E). If standalone energy devices are installed in your home, the Energy Center will be available to help you manage and monitor your energy usage.

Standalone Energy Devices:

  • EVlink Home Smart

  • Schneider Charge

  • Wiser Power Micromodule

  • Connected Single Socket Outlet 16 A

  • PowerTag Energy

  • Wiser Plug

In the Energy Centre, you can monitor your energy production, view detailed consumption history, and track energy costs by entering your tariff.

IMPORTANT: The Wiser system supports the configuration with the following energy source and combinations:
  • No Sources

  • Solar

  • Battery

  • Solar + Battery

To navigate to the Energy Center:

  1. On the Home Screen, tap .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?