SUG_Wiser_Home_Iberic_WH-05

Insights

The Insights feature gives you multiple features in a single place. This includes energy saving, system activity, heating time and access to your heat report.

To navigate to Insights from the Home screen:

  1. Tap Insights (A)

NOTE: If you have an energy device or energy monitoring device installed at your home, Energy Center will be displayed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?