SUG_Wiser_Home_Iberic_WH-05

Wiser Home AI

Wiser Home AI is a feature that allows users to save electricity costs by enrolling high energy devices like EV Charger (EVlink Home Smart, Schneider Charge, EVlink socket) or resistive Water boilers (controlled with a micromodule). It is used with variable tariffs, such as peak/off-peak tariff, and relies on users to answer routine questions. The Al creates smart schedules for enrolled devices and limits the usage of these devices when electricity prices are high, while following user’s habits. It adapts the last 30 days of consumption data from the Grid.

  • Savings on electricity bills upto 10 %

  • If you have installed and configured solar panels in your home before opting for Wiser Home AI, you can save up to 50% on your electricity bill.

  • Your savings will be monitored on a daily, monthly and yearly basis.

IMPORTANT:
  • The AI system learns by itself and benefits from historical data on electricity consumption. It can already optimize to some extent without pre-existing data, and its performance will improve significantly over time.

  • While this feature is active, Wiser Home AI schedules replace any customized schedules.

  • You can enroll upto two different devices - 1 EV device and 1 Water Heater.

Supported devices:

  • Power Micromodule (Water Heater)

  • EVLink Home Smart

  • Schneider Charge

Pre-requisite

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?