SUG_Wiser_Home_Iberic_WH-05

System Requirements

For a Wiser system you need at least the following devices and conditions.

Wiser Hub

The Hub communicates with all Wiser devices and the Wiser Home app.

You can find more information about the available hubs in Chapter List of Wiser Devices

Internet access for the Hub

In order to properly control Wiser Devices, the hub needs to be connected to the internet via your router.

IMPORTANT: The hub requires IPv4 network features to function correctly. To ensure full functionality, make sure that IPv4 is enabled in your local area network and internet settings on your internet provider’s router. Systems configured as IPv6-only will impact your hub’s ability to communicate and receive software updates, and may affect your ability to remotely control the hub.

Wiser devices

You can find more information about the available Wiser Devices in Chapter List of Wiser Devices

Smartphone

iOS Version 12 and higher

Android Version 5 and higher

Wiser Home App

For more information, please read chapter Downloading the Wiser Home App.

A valid e-mail address.

To set up your Wiser system, you will need to register an account at Schneider Electric with a valid e-mail address.

Data localization

Data Localization in general refers to a mandatory legal or administrative requirement directly or indirectly requiring that data be stored or processed, exclusively or non-exclusively, within a specified jurisdiction.

If data localization laws apply in your region, we strongly recommend setting up this device or system in a way that would not conduct a data cross-border transfer directly or through other channels. Details of data localization laws may vary in different regions. Your legal team is the best resource to give you compliance advice for your specific situation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?