DUG_Temperature/Humidity Sensor_WSE_02

Using the device

On the Home page, tap All devices > Temperature Humidity Sensor to access the control panel.

On the Sensor control panel page, you can see the following:

  • Battery level (A)

  • The current temperature value (B)

  • The current humidity value (C)

  • History (D)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?