DUG_Temperature/Humidity Sensor_WSE_02

Example of an automation

This demonstration shows you how to create an automation to open the shutter when the room is warm.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name, enter the name of the automation and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping .
  3. Tap Add Condition > When device status changes > Temperature Humidity Sensor.
  4. Tap Current temperature, set the temperature and condition and tap Next.
    TIP: You can set the temperature as 27 °C and the condition as > (greater than).
    NOTE: The automation is triggered only if the status of the Sensor changes to a higher temperature than the set temperature. In this case, the automation is triggered when the temperature changes from 27 °C to 28 °C.
  5. Tap to add another condition and tap When device status changes > Temperature Humidity Sensor.
  6. Tap Current humidity, set the humidity and condition and tap Next.
    TIP: You can set the humidity as 65% and the condition as > (greater than).
    NOTE: The automation is triggered only if the status of the Sensor changes to a higher humidity than the set humidity. In this case, the automation is triggered when the humidity changes from 65% to 66%.
  7. Tap Add task > Run the device > Shutter.
  8. Tap Control (A), select Shutter Open and tap Save.
  9. Tap Percentage (B), set the shutter open percentage and tap Save.
  10. Tap Next.

  11. In the Automation Settings page, tap Save.

    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?