DUG_Temperature/Humidity Sensor_WSE_02

About the device

The Wiser Temperature/Humidity sensor (hereinafter referred to as sensor) combines two sensors in one unit. The sensor measures temperature and humidity in the environment where the sensor is installed. When the sensor is connected to the Wiser Gateway, it reports the temperature and humidity data to the Wiser Gateway.

The sensor triggers other Wiser devices (such as turning on an air conditioner if the temperature is high or turning on an exhaust fan if the humidity is high) through automation.

Operating elements

  1. Status LED

  2. Function key

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?