DUG_Temperature/Humidity Sensor_WSE_02

Pairing device with auto scan

Pairing the device with auto scan automatically discovers the device when the corresponding device is powered on.
To pair the device:
  1. On the Home page, tap +.
  2. Tap Auto scan and than tap Confirm.
  3. If you have multiple hubs, do Step 4 or proceed to Step 5.
  4. Tap Select hub and select the Wiser hub from the slide-up menu.
  5. Short press the function key 3 times (< 0,5 s).
    NOTE:
    • The LED blinks orange.

    • Wait for a few seconds until the device search is complete.

    TIP: If you want to pair multiple devices, perform step 5 on each device and wait for a few seconds.
  6. Select Temperature Humidity Sensor and tap Next (A).

  7. Tap Done when the pairing is successful.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?