DUG_IR Converter_WSE-01

Changing the device location

You can change the device location using the Wiser app.
  1. On the Home page, select the device for which you wish to change the location.
  2. At the top-right corner of the screen, tap .
  3. Tap edit next to the device name.
  4. Tap Location.
  5. Select the desired location from the list (A) and then tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?