DUG_IR Converter_WSE-01

Resetting the device

You can reset the device to factory default manually.
To reset the device:
  1. Short press the S/R button three times (< 0.5 s) and then long press the push button once (>10 s).
  2. After 10 s, LED starts blinking red then release the push button.
  3. The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts and the LED stays orange before turning Off.
    The LED stops blinking upon successful reset of the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?