DUG_IR Converter_WSE-01

About the device

The Wiser IR Converter (or IR Convertor) is a control device to automate your home infrared (IR) controlled devices such as televisions, air conditioners, music systems and so on. The device converts mesh network signal to infrared signal.

Key features

  • 360° IR signal coverage

  • 3 sockets for IR extension cables

  • Supports up to 8 types of IR controlled devices

Operating elements

  1. Set/Reset button

  2. Network status LED

  3. IR LED

  4. 3× 3.5 mm phone jacks for IR extension cables

  5. Micro USB port for 5 VDC power supply


Suitable install location

IR Convertor can be placed on table or mounted on ceiling to provide desired coverage:

  • Placed on a table provides a surrounding 360° IR signal coverage with a maximum control distance of 8 m.

  • Ceiling mount provides a surrounding 180° IR signal coverage with a maximum control distance of 8 m.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?