DUG_Exxact verhokytkin_WH-00

Changing the orientation of outside temperature sensors

You can change the orientation of the outside temperature sensors in the Wiser Home app.

To change the orientation of the outside temperature sensors:
  1. In the Seasonal Comfort Mode set-up page, tap Outside temp sensors.
  2. Tap to see the available outside temperature sensors in Wiser Home app.
  3. Select the orientation in which the outside temperature sensors are facing and tap Set.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Auttoiko tämä?