Shutter calibration with Wiser app
-
It is necessary to select the device type and set the default run time before proceeding with shutter calibration. Refer to Selecting device type and Setting default run time .
-
Do not use the shutter either manually or on the app during calibration to avoid interruption.
-
Follow the procedure for shutter calibration according to the device type: Shutter or Shutter with tilting slats.
Shutter
-
Upon setting the default run time, go to the Control tab, tap All devices or the room tab where the device is located.
-
On the device control screen, drag the sliding bar up/down to set the desired shutter opening percentage (A).
The shutter opens completely and then it reaches to the desired position set in step 2. The shutter is now calibrated.
Shutter with tilting slats
-
On the Control tab, tap All devices or the room tab where the device is located.
-
On the device control screen, in the Position tab, drag the sliding bar up/down to set the desired shutter opening percentage (A).
-
Tap Slat Tilt
tab, drag the sliding bar up/down to set the desired shutter opening percentage (B) according to any one of the following tilt position:-
Horizontal
-
Tilted
-
Vertical
-