DUG_Exxact Multiwire Rotary Dimmer_WH-00

Switching/Dimming the device manually

You can manually turn ON/OFF the dimmer and increase/decrease brightness level. This will provide power to the load connected to it.
Short press the push button (< 0,5 s) once to switch ON/OFF the dimmer.

To increase brightness, turn the dimmer knob clockwise, and to decrease brightness, turn it anti-clockwise.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?