DUG_Exxact Multiwire Rotary Dimmer_WH-00

Adjusting the brightness level using app

By using the Wiser Home app, you can increase/decrease the brightness level of the dimmer.
  1. On the Control tab, tap All devices or the room tab where the dimmer is located.
  2. On the Device Control Screen, drag the sliding bar up/down to increase/decrease the brightness (A).
    TIP: You can also turn On/Off the dimmer on the Device Control Screen, tap (B) to turn On/Off dimmer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?