DUG_LK FUGA Wiser wireless PIR dimmer with neutral_WH-01

Away Mode

Away Mode automatically turns off the Motion Sensor Dimmer. For example, when you are away from home for a long time, the light should not turn on due to false motion detections. This feature ensures the device remains off even if motion is detected, helping to save energy.

  1. On the Home screen, tap > Away Mode.

  2. Under the LIGHTS section, tap the Motion Dimmer (A) toggle to add it in Away Mode.

TIP: For more information on Away Mode, refer to the Away Mode topic in the respective System User Guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.