DUG_LK FUGA Wiser wireless PIR dimmer with neutral_WH-01

About the device

The LK FUGA® Wiser wireless PIR dimmer with neutral (hereinafter referred to as Motion Sensor Dimmer) detects moving heat sources (e.g. persons) and can dim ohmic, inductive or capacitive loads and switch them on for a settable overtravel time.

Control options

Home control: To control the motion sensor through the Wiser Home app you will need the Wiser Hub.

Direct operation: The motion sensor can always be controlled directly on-site. You can also connect any number of mechanical push-buttons to control the device.

Functions

  • Automatic load detection.

  • Thermal protection, overload-resistant, short-circuit protection, soft start, soft stop.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?