DUG_LK FUGA Wiser wireless PIR dimmer with neutral_WH-01

Setting the detection sensitivity

You can set the sensitivity level of the sensor.
  1. On the Home screen, tap .
  2. Tap Devices > Lights > Motion Dimmer > Motion Detection Sensitivity and select any one of the following options:
    • Low: Detects only larger or closer movements (for example, a person walking near the sensor).

    • Medium: Detects normal human movements at a moderate range.

    • High: Detects even small or distant movements (for example, a pet walking by or a curtain moving).

    TIP: Tap to view information about Motion Detection Sensitivity.
    NOTE: Sensitivity is set to High by default.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.